Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
magjack-slide2

IEEE 802.3 is a collection of IEEE standards defining the physical layer (PHY) and the media access control (MAC) of wired Ethernet connections. Designs based on the IEEE 802.3 standard allow interoperability between components from various vendors.  Each component in the system is necessary to allow generic computer A to communicate with generic computer B. The MagJack® is an important component of the overall IEEE 802.3 Ethernet puzzle.

PTM פורסם ב: