Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Shadow HBC Series Connectors Slide 5

The HBC feed-thru BNC connector was engineered from the contact up to meet the rigid standards of HDTV. This uniquely designed true 75Ω panel connector was developed to perform well at frequencies in the range of 100 MHz to 3.2 GHz. The feed-thru is panel isolated and has a black anodized nickel plated bushing and flange that helps identify the connector as one of the Shadow™ HBC series high definition connectors.

PTM פורסם ב: