Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
AMS22B-Slide2
The Bourns® Model AMS22B Rotary Non-Contacting Position Sensor is the latest product in a new line of Bourns® electro-mechanical sensing products based on non-contacting magnetic sensor technology. The core of this rotary position sensor is a programmable quad Hall effect IC that provides a signal which is converted into a voltage output. The Model AMS22B Rotary Non-Contacting Position Sensor is programmed at the factory to meet any rotational angle between 10° and 360°. It is especially well-suited for harsh environments and long life applications.
PTM פורסם ב: