Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
motor and drive
In addition to motor drives used in factory automation, there are many other applications. Machine tools and pumps are just two examples. As mentioned in the previous slide, MOSFET / IGBT and IPM couplers are used to isolate the control circuit from the high-power motor circuit. Isolation amplifiers are used in the feedback loop of a motor to the control circuit.
PTM פורסם ב: