Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
SealedSwitchPt4-Slide9

The CF threaded, splash proof IP67 sealed bushing has an internal O-ring and a standard external bushing seal washer. The external bushing seal is placed on the switch. The switch is then inserted into the panel and the mounting nut is applied. Once installed the switch is IP67 sealed above the panel. They are designed to be used in Hand-held telecommunications, Instrumentation, and Medical equipment applications.

PTM פורסם ב: