Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
Sealed Power Plugs and Jacks Slide 6

The most common applications for the new Switchcraft® sealed power plug and jack are in mobile equipment that is frequently placed in demanding environments. This can include medical devices which frequently need power supplies that are mobile. Also, medical applications need protection from fluid spills and other items that could interrupt power to a device, so it is critical to make sure that these potential power interruptions are eliminated, hence the use of a high quality sealed power plug and jack from Switchcraft. Another common application is outdoor control equipment. More and more frequently the control unit for equipment is being moved to the location of the equipment itself which means that the control unit needs to withstand the same environment as the typical working environment of the equipment; which can mean dirt, dust and moisture. With the Switchcraft sealed power plug and jack power can be brought securely to any piece of equipment even when that environment has water or dirt which are often a limiting factor to continuous operation.

PTM פורסם ב: