Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
output waveform
This slide shows the output waveforms of the JT22 and JT30 potentiometers. Within the effective electrical angle, output voltage will go up to 4.5 V as the shaft rotates clockwise to the limit effective electrical angle, and then go down to 0.5 V as it rotates counterclockwise to the opposite limit. The shaft can be rotated 360° continuously and certain output voltage is generated outside effective electrical angle. However, such output voltage is unstable and not specified properly. The customer should use output voltage within effective electrical angle.
PTM פורסם ב: