Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
TFSeries-Slide12

In summary, Nidec Components' TF series Micro Blowers are compact, lightweight, and able to create a high static pressure. The unique aero-dynamic bearing enables these blowers to have a long life and low vibration because there is no wear between the sleeve of the impeller and the shaft of the blower. These bearings are not affected by normal temperature changes and are environmentally friendly as they do not need to use oil for lubrication between the shafts and sleeves. They are ideal for medical devices, industrial equipment, home appliances, data storage servers, and printing machines. Nidec Components also offers development support kits and drivers to help shorten evaluation and product development time.

PTM פורסם ב: