Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
Slide13
Here is a platform overview of the CXA CRI 95 offering. In neutral white, the High CRI options are still above 92 Lumens per watt at 85°C. In warm white, at 85°C the High CRI option is still above 80 lumens per watt for the 15, 18, and 25 Series and 88 lumens per watt for the 30 Series, which are industry leading levels of efficacy for a high CRI Solution.
PTM פורסם ב:
PTM Updated on: 2023-01-19