Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
millenium-slide4

At this point the user will see a window pop up next like the one shown on the upper left.  Click on the Download zip button. The user will then be asked to either open or save the file. Select “Save” and choose the folder in which the file will be stored. The file will begin downloading like below.  Now the user is ready to start the installation.

PTM פורסם ב: