Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
snap-action-slide16

In summary, there are many mechanical and electrical components to consider when choosing a snap-action switch: Electrical function/ Circuit diagram, Current rating/ Breaking capacity, Housing type and size/ fixing mean, Terminal type, Actuator type, Force, position and travel requirements, Ambient temperature, Degree of protection, Shock and vibration resistance. If one of these standard snap-action switches does not meet the customers needs, full switch customization is also available.

PTM פורסם ב: