Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Quartz Crystal Resonators Slide 12

The terms accuracy, stability, and precision are often used in describing an oscillator's quality. This slide illustrates the meanings of these terms with respect to a marksman and a frequency source. Accuracy is the extent to which a given measurement, or the average of a set of measurements for one sample, agrees with the definition of the quantity being measured. It is the degree of "correctness" of a quantity. Reproducibility is the ability of a single frequency standard to produce the same frequency, without adjustment, each time it is put into operation. From the user's point of view, once a frequency standard is calibrated, reproducibility confers the same advantages as accuracy. Stability describes the amount something changes as a function of parameters such as time, temperature, shock, and the like. Precision is the extent to which a given set of measurements of one sample agrees with the mean of the set.

PTM פורסם ב: