Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
 The Human Ear and A-Weighting

The 20Hz to 20kHz range tends to be the general range for human ears. This range is reduced with age, especially in males. In older males 13 kHz tends to be the upper end of the audible range. The human ear does not have a flat frequency response over the audible range. Certain frequencies tend to be attenuated while others are magnified. A-weighting attempts to compensate for this by discounting frequencies which the human ear is less sensitive to. It places priority on sounds between 1kHz and 7kHz. Some Same Sky speakers specify SPL using the A-weight system, also known as dBA.

PTM פורסם ב: