Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Bluetooth 4.2 Overview Slide 9

Using the BLE component in Creator, the complex BLE protocol stack can be configured in minutes, and a first data transfer can happen quickly. First, open the BLE component configuration tool, select the application profile, all of the BLE SIG adopted profiles are already available in the component, and nothing needs to be implemented from scratch. Then, configure the GAP and the peripheral rules, configure the selected profile, configure the GAP settings, access the BLE APIs from the component datasheet, and then easily write application firmware logic. In short, all of the protocol complexity is taken care of by the BLE component configuration tool so the application glue logic can be focused on.

PTM פורסם ב: