Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Energy Harvesting PMIC Portfolio Slide 11

In summary, Cypress provides the world’s lowest-power, single-chip Energy Harvesting PMIC solution for tiny, solar-powered WSN IoT Devices. With Moore's Law driving semiconductor per-feature cost down, sophisticated processing and sensing capabilities are being pushed out further and further from centrally located computers. New devices with these capabilities collectively called Internet of Things, or IoT, devices are expected to explode in numbers over the next five years across all vertical applications markets. An IoT device is simply connected embedded systems, that are remotely installed. Wireless sensor nodes are the most common of these devices, combining sensors and processing in a single device. All of these devices have the following technology needs: first of all they need wireless connectivity, most often Bluetooth Low Energy due to low power requirements. They also consume very low amounts of power and often are self-powered by Energy Harvesting from the environment through light, motion, or heat, thereby eliminating the need for battery maintenance. Lastly, they often have a very small form factor. Cypress offers IoT device designers a one stop shop for their Energy Harvesting IoT device semiconductor needs, with memories, interfaces, MCUs, wireless connectivity, and power products.

PTM פורסם ב: