Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
SPI Guide Data Protection Interfacing SPI

Shown on this slide is an example of a F-RAM solution in an automotive infotainment system. As a recap, F-RAM requires no Soak Time to write data, requires no additional capacitors or batteries to complete Page Write low-power loss, and provides endurance of 100 trillion write cycles. Additionally, it offers AEC-Q100-qualified memory components in volume. To get started, the designer can take a look at the detailed application notes.

PTM פורסם ב: