Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
PSoC 4 Solution for Thermal Management Slide 7

A thermal management system design is not simple. The Thermal Management example project provides PSoC Creator components that integrate common Thermal Management ICs and that are customized by the Component Configuration Tool and prototyped and validated using the PSoC 4 Pioneer Kit, PSoC Shield adaptor Kit, and the Thermal Management Kit to create a one-chip customized fail-safe thermal management solutions. To get started with this design cycle, the customer should download the PSoC 4 Fan Controller Application Note, which includes the Thermal Management Example Project. The PSoC Creator software will be needed on a PC, and the pioneer kit (CY8CKIT-042), the PSoC shield adapter kit (CY8CKIT-019), and the thermal management kit (CY8CKIT-036) should be purchased. Open the thermal management example project and PSoC creator and use the fan control app note for complete system design guidelines.

PTM פורסם ב: