Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
CPU-Slide6

A heat pipe is a heat transfer mechanism that combines the principles of both thermal conductivity and phase transition to efficiently manage the transfer of heat between two solid interfaces. At the hot interface within a heat pipe, which is typically at a very low pressure, a liquid in contact with a thermally conductive solid surface turns into a vapor by absorbing heat from that surface. The vapor condenses back into a liquid at the cold interface, releasing the latent heat. The liquid then returns to the hot interface through either capillary action or gravity action where it evaporates once more and repeats the cycle.

PTM פורסם ב: