Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Slide3

The frequency generator function produces a square wave signal with a frequency that is proportional to the fan speed. This enables the system to detect situations such as low supply voltage or a partially blocked air flow. The frequency generator output is an open collector NPN transistor with a 5 mA max collector current.

PTM פורסם ב: