Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
ZigBee in a Nutshell Slide 5

A mesh network is a topology in which each node in the network is connected to other nodes around it. Each node cooperates in the transmission of information. Mesh networking provides three important benefits: routing, ad-hoc network creation, and self-healing. With the routing technique, the message is propagated along a path by hopping from node to node until it reaches its final destination. Ad-hoc network creation is an automated process that creates an entire network of nodes on the fly, without any human intervention. Finally, self-healing; this process automatically figures out if one or more nodes on the network is missing and reconfigures the network to repair any broken routes.

PTM פורסם ב: