Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List Associated Content
Gate Driver Slide 2

Initially the designer will need to specify the selection and/or design in criteria. This includes: The number of inputs and outputs that are required for the application, the maximum voltage rating required by the application, the maximum drive current rating required by the application, and any special functions that the gate driver must offer. Finally, key external components can be specified to optimize the design.

PTM פורסם ב: