Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Slide5

EC motors are capable of speed control from 10% ~ 100% of the maximum speed. Since the power required by a fan has a cubic relationship to the speed at which the fan is running there are substantial savings available by speed controlling a fan to a lower RPM. If multiple fans are set up in parallel there are large savings from speed controlling the fans instead of using on/off operation.

PTM פורסם ב: