Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
moving-air-slide10
When the application requires DC input, a brushless DC motor will typically be used.  A brushless DC motor, also known as an EC or “Electrically Commutated” motor, uses an electronic circuit and permanent magnets to generate rotation. The end result is a highly efficient and highly reliable motor. The commutation electronics are typically built right into the motor so the user only needs to apply DC voltage to the motor.
PTM פורסם ב: