Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
therm trig1
EPCOS developed the ETFV series Varistors to satisfy the requirements of a TVSS module to UL 1449, Section 37 (abnormal overvoltage limited current requirement). The UL 1449 standard specifies that the ThermoFuse, in the thermally protected varistors, must be triggered by a current of 0.125A. During an extreme overvoltage, the solder melts and the ThermoFuse opens.
PTM פורסם ב: