Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
SAW-Slide12

Shown here is a phase noise comparison of an Epson SAW oscillator, an analog-multiplier XO and a PLL-based XO at 622.08 MHz. Epson SAW oscillators have excellent close-in and noise floor characteristics since it can be driven at a higher drive level. The analog-multiplier XO’s noise floor has sub-harmonic spikes while the PLL-based XO’s noise floor is greatly deteriorated by the PLL multiple of the spurious noise. The Epson SAW oscillator does not have sub-harmonics nor spurs affecting the phase noise, and the structural reliability is not affected even with the higher drive level.

PTM פורסם ב: