Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
powerxr-slide17

The XRP77xx PowerXR part is an un-programmed, adjustable part. The designer puts it in the system, the system powers up, the standby linear regulator turns on, it powers a micro controller, the microcontroller loads the memory from some Flash or external Flash, the part powers up and the system is up and running. This would allow the designer to use a single part in inventory, as a result reducing inventory and allowing flexibility.

PTM פורסם ב: