Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
NerOCleO-Slide13

A second example is included on this slide to highlight the ease at which video can be captured and displayed. All that is required to display captured video on the CleO is the use of one instruction, CleO.RecorderPreview(). A camera accessory which plugs directly into a connector on the CleO PCB is available for purchase from DigiKey, this is shown on the following slide.

PTM פורסם ב: