Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
therm grease
Thermal greases are known as the “traditional” TIM material, and is typically a silicone filled with thermally conductive filler. Greases have been around for decades as a commoditized product for the PC industry. This is because they provide good overall thermal performance at a low cost. However, thermal greases are messy to work with and difficult to clean. Also, they can potentially pump-out of interfaces if cycled too frequently. This can result in decreased reliability and thermal failure.
PTM פורסם ב:
PTM Updated on: 2017-06-14