Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
function
Why should the air be replaced? Air is a poor thermal conductor, with thermal conductivity of only 0.026 W/m*K. TIM materials have thermal conductivity nearly 20 times higher than air, or greater than 0.5 W/m*K. The other function of a TIM is to minimize thermal resistance to the hot surface by maximizing wetting and surface area.
PTM פורסם ב: