Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
idc female
The Archer IDC cable-to-board option provides cable connection to 0.635mm pitch flat 30AWG ribbon cables. IDC contacts make connection to the wire by cutting through the insulation as part of the process of wire assembly to the connector. Therefore, no wire stripping is required, making the Archer a fast, single-operation connector.
PTM פורסם ב:
PTM Updated on: 2017-10-19