Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
DF57-Slide5

The unique locking structure actually strengthens as a tension load is place in the direction of the wires. Accidental un-mating if the wires are pulled upward is resisted up to 5 Newtons, but will not result in significant damage to the connector if over ridden. The mating sequence is begun by first pressing the rear, wire end, of the connector into the slots of the header body.

PTM פורסם ב: