Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
DF59S-SN-Slide7

Also available is the super slim plug DF59SN. This connector width is only 1.7mm as compared to the 2.7mm width of the DF59S. The DF59SN uses a common receptacle as the DF59S as well as the same floating action. Please make sure to keep sufficient insulating distance around the connector due to the exposed contact.

PTM פורסם ב: