Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
DF62-Slide9

The DF62P is the panel mount type plug that is also available. Easy to use, the DF62P plug is mounted to the panel by pushing it into the panel cut-out, and is retained in place by integral mounting fingers. Mounting is complete once it snaps into place. The DF62P uses the same terminals and socket as the DF62; there are no parts other than the housing that are unique to the DF62P type.

PTM פורסם ב: