Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Image of Honeywell NBP Series

There are numerous medical applications the Basic Board Mount Pressure Sensors may be potentially used in. For example, they can be used to monitor the air pressure in hospital beds so that the desired firmness can be controlled, helping improve patient comfort and reducing bedsores by alternating pressure to various zones. They can also be used to monitor the pressure internally in the sieve bed in oxygen concentrators so that the sieve bed can generate the required oxygen levels for the patient. This helps enhance system response time and minimize oxygen use when the patient is not inhaling. The sensor may also potentially be used in wound therapy machines to monitor the pressure applied to the wound via the suction system. This can help provide maximum therapeutic effect without causing the patient harm.

PTM פורסם ב: