Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Zephyr-Slide8

Another important feature is that these sensors offer bidirectional flow sensing capabilities that eliminate the need to have two sensors to detect airflow in both directions, helping to reduce space, production costs and implementation size. Additionally, these devices are insensitive to mounting orientation and altitude, important for applications where one has to mount the sensor in a space-constrained area, or at high elevations. Finally, these sensors are RoHS compliant.

PTM פורסם ב: