Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Zephyr-Slide5

The second of the six advantages is a Wide airflow range. Zephyr™ Airflow Sensors are able to detect the presence or absence of airflow from ±50 SCCM to ±750 SCCM. This allows customers that have already designed a bypass the ability to choose an airflow sensor to optimize their overall performance. The lower flow range sensors have high sensitivity which can help optimize performance in industrial applications such as gas leak detection and clogged HVAC air filter detection. Likewise, the higher airflow ranges can increase the ability to integrate the sensor into applications that require higher flows.

PTM פורסם ב: