Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
cr
The C+R mode is the capacitance on the primary display and the parallel resistance R is shown on the secondary display. In AUTO mode, the Smart Tweezer first tries to perform measurement at 1 kHz and then automatically selects the best test frequency. The device is capable of measuring capacitance from approximately 3 pF to 199 μF in AUTO mode. To measure capacitance lower than 4 pF, select the 10 kHz test frequency manually. To measure capacitance higher than 200 μF, use 100 Hz or 120 Hz.
PTM פורסם ב:
PTM Updated on: 2019-02-26