Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Image of InnoSenT IMD-2000 Radar Motion Detector - IMD-2000

Since the company was founded in 1999, InnoSenT has been developing radar-based motion detectors for industrial applications. Now InnoSenT radar experts would like to introduce a new radar sensor for motion with extended functions that will dominate the motion sensor market. The IMD-2000 is a 24GHz radar sensor which offers motion detection with ranging. Its features enable increased efficiency due to more object data and easily configurable options. The sensor resolves velocity, distance, and direction of moving objects. Users can configure the distance up to 50 meters and filter out unnecessary detections by RCS and range. It outputs a target list via UART. With the IMD-2000, InnoSenT has implemented all the current requirements for motion detection and combined it with the advantages of radar technology in order to bring motion sensor applications to the next level. The product can be used for various applications as a trigger, especially automation and security applications that may be optimized with reliable radar detection.

PTM פורסם ב: