Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
FSR-Slide3

For best results, the seven steps shown on this series of slides should be followed when beginning any new product design, proof-of-concept, technology evaluation, or first prototype implementation. The first step is to start with reasonable expectations, to know the sensor. The FSR sensor is not a strain gauge, load cell, or pressure transducer. While it can be used for dynamic measurement, only qualitative results are generally obtainable. Force accuracy ranges from approximately ±5% to ±25% depending on the consistency of the measurement and actuation system, the repeatability tolerance held in manufacturing, and the use of part calibration.

PTM פורסם ב: