Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Slide19

This slide captures thermal performance data collected using the competitor’s solution on the left vs. the Renesas digital multiphase controller paired with the 60 A ISL99227 Smart Power Stage on the right using a FLIR thermal camera. To support testing, a thermal wind tunnel was utilized to collect data at 75°C ambient conditions using 200 LFM airflow. For this analysis, both Renesas and the competing solutions were subject to the same test conditions. A FLIR thermal camera was used to measure controller, SPS, and inductor current information. As evidenced in the thermal images captured, the competing solution must de-rate current by 30% for comparable thermal performance with the Renesas SPS at Tj = 106°C. 

PTM פורסם ב: