Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Slide12

Configuration 3 has the RS-485 transceiver configured for half-duplex operation, which requires only two conductors for long-haul networks. Note that for long distance transmission lines the RS-485 transceiver should be set to slow-mode (115 kbps). The RS-232 receiver controls the operation mode of the RS-485 transceiver. A low at R1OUT (and hence at DI) sets the RS-485 transceiver into transmit mode by enabling the driver and disabling the receiver. A low at DI is therefore actively converted into a negative bus voltage. A high at R1OUT accomplishes the opposite and switches the RS-485 transceiver into receive mode. With the driver outputs now being high-impedance, a positive bus voltage is established by the failsafe biasing resistor network. The small deglitch circuit consisting of an inverter and a R-C-D unit prevents the occurrence of glitches on the bus during the transitions from drive into receive mode. This half-duplex level translator is the most efficient of all, as it saves an entire conductor pair versus a full-duplex level translator, and also frees up the second RS-232 channel, which can now be used for other interface purposes.

PTM פורסם ב: