Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
SM3-Slide4

The SM3 series allows the card to be inserted at a slight angle in order to reduce the insertion and extraction force required during assembly or replacement of the card. Once the card is fully inserted, it should be fixed in place so that it is parallel to the main PCB which the connector is mounted on.

PTM פורסם ב: