Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
ST11-Slide10

In summary, JAE’s ST11-H series is a push-push type connector compatible with the microSD card, which is standardized by SDA (SD Card Association) as a compact card for hand-held devices. Its structure includes a card insertion detection switch, which is normally a closed type, a balanced EMI countermeasure with 7 hold-down points and a structure built to prevent the card from popping out. There is growing demand for microSD cards for use in smartphones and tablets. The ST11-H series is also lead free and halogen free compliant product that supports automated mounting.

PTM פורסם ב: