Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Image of KEMET Ceramic Capacitor Basics Pt 2 - IR

The second topic in this product training module is insulation resistance. In this slide, an ideal capacitor is shown with two conductive electrodes separated by a perfectly insulative dielectric material. However, a real capacitor will have Ohmic losses due to imperfections in the dielectric material. This creates a finite resistance in parallel with the capacitor and is known as the insulation resistance. The values of insulation resistance for ceramic capacitors range from the low mega-Ohms to hundreds of tera-Ohms. For almost all applications, higher insulation resistance is always desirable.

PTM פורסם ב: