Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Image of KEMET Ceramic Capacitor Basics - Dielectric Classification Continued

Class 2 and Class 3 dielectrics are specified differently using their three characters. Because Class 2 and Class 3 dielectrics are not as stable as Class 1, their capacitance change is given in percent and not ppm per degrees Celsius. The first character defines the minimum operating temperature. The second character defines the maximum temperature range. The third character defines the maximum change in capacitance over the entire operating temperature range. For example: X7R has an operating temperature of -55°C to 125°C with a maximum capacitance shift of plus or minus 15% over that operating temperature range.

PTM פורסם ב: