Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
High Performance X2 Film Capacitors, the F862 Series Slide 18

In summary, KEMET’s F862 is quite suitable for applications in series to the mains and/or in parallel to the mains as well as in harsh environmental conditions. One more point that can be highlighted here is that in order to achieve such performances no impregnation is required.

PTM פורסם ב: