Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
KOCAP-Slide10

The power capability for these capacitors is dependent on the ESR and the physical structure of the package to conduct heat from the pellet structure. A facedown package (thermal resistivity of 44°C/W for the T528, and 160°C/W for the T520) can stay cooler with more power passing through it. To achieve +20°C temperature rise at 1MHz, the T520 would be restricted to 4.74Arms (125mW), while the T528 will allow 8.73Arms (450mW).

PTM פורסם ב: