Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List Associated Content
basic with VIM

The Tone Board can be used in two ways. The first is by connecting it with a Khadas VIM single board computer that can be ordered from DigiKey using the part numbers starting with KVIM1 and KVIM2 (ex. KVIM1-x-002 and KVIM2-x-002). It supports S/PDIF IN and OUT, and has reserved interfaces such as I2C, I2S, and ADC. Power and audio data will be supplied from the Khadas VIM SBC.

PTM פורסם ב: