Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Image of Kingston Technology IronKey Encrypted USB and External SSD Solutions - Keypad 200

The IKKP200 is a small form-factor keypad drive. It is one of the first drives in the industry to have passed the FIPS 140-3 Level 3 certification testing by a NIST-certified lab, however, it is listed as “pending” as NIST must review the lab testing results and provide Kingston with an official certificate. It has brute-force and BadUSB attack protection, as well as multi-PIN options. It also has a global and session Read-Only modes that can be used to protect the drive from malware or accidental changes by a User. This is most useful when sharing the drive with others to ensure that it cannot be changed accidentally or have injected malware. This drive can be used in conjunction with the IKVP80ES for use cases where lower capacity and portability are more important.

PTM פורסם ב: