Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Measuring the Frequency Response of Balanced Armature Drivers and Earphones Slide 8

The IEC 711 coupler is also used to measure earphones when paired with the DB2012 interface. In fact it is the only recognized standard for taking in-ear earphone response measurements. It has the same issue with respect to resonant frequency, often showing up as an artificial peak in the 8 to 12 kHz range depending on the earphone.

PTM פורסם ב: